| 1974 | 
                Establishment of the Company on 3rd of July  | 
              
              
                | 1975 | 
                Construction of the first building completed | 
              
              
                | 1976 | 
                Commemoration of first shipment of TO92 Transistor | 
              
              
                | 1977 | 
                Construction of the second building completed | 
              
              
                | 1979 | 
                Introduction of Integrated Circuit (IC) Package | 
              
              
                | 1981 | 
                Construction of the third building completed | 
              
              
                | 1987 | 
                Construction of the fourth building completed | 
              
              
                | 1994 | 
                ISO 9002 Certification | 
              
              
                | 1997 | 
                Construction of the fifth building completed 
                  Introduction of QFP 44P Matrix | 
              
              
                | 1998 | 
                ISO 14001 Certification | 
              
              
                | 1999 | 
                Launching of TPM | 
              
              
                | 2002 | 
                ISO 19001 Certification (upgraded version) | 
              
              
                | 2003 | 
                TPM Excellence Award | 
              
              
                | 2004 | 
                TS16949 Certification | 
              
			
                | 2010 | 
                NEC Electronics merged with Renesas Technology on 1st Apr | 
              
			  
			 
                | 2014 | 
                SAP System Introduction & RSS Transfer Project | 
              
 
			  
			  
			    | 2015 | 
			    SAP System Go Live | 
		      
			  
			    | 2016 | 
			    SAP System Go Live  | 
		      
			  
			    | 2017  | 
			    In House Plating  | 
		      
			  
			    |   | 
			    ISO 14001 : 2015  (upgraded version) | 
		      
			  
			    | 2018     | 
			    IATF 16949  Certification | 
		      
			  
			    | 2019   | 
			    Smart Factory Level 1  |